Operator ImageStatistics measures frame properties for whole frame sequences without touching the image data.
Operator ImageStatistics analyzes image sequences. For analyzing individual images, use operator Operator ImageAnalyzer.
The operator allows to analyze deviations between frames (width, height, size, line gaps, etc.). The operator also provides measurands regarding line rates and frame rates.
In addition, operator ImageStatistics provides data about the utilization of the pipeline capacity (valid fraction, idle fraction, blocked fraction of time in percent).
When an internal counter overflows, a corresponding overflow bit is set in the OverflowMask parameter and the counter halts.
![]() |
Runtime Testing |
---|---|
This operator is designed for testing and analyzing your design during runtime: You need to build (synthesize) the design, load it onto the target hardware, and start actual image processing, before you can use the operator for debugging. The operator is not intended for design simulation within VisualApplets. |
Property | Value |
---|---|
Operator Type | O |
Input Link | I, image data input |
Output Link | O, image data output |
Link Parameter | Input Link I | Output Link O |
---|---|---|
Bit Width | [1, 64] | as I |
Arithmetic | {unsigned, signed} | as I |
Parallelism | any | as I |
Kernel Columns | any | as I |
Kernel Rows | any | as I |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D} | as I |
Color Format | any | as I |
Color Flavor | any | as I |
Max. Img Width | any | as I |
Max. Img Height | any | as I |
ClearMode | |
---|---|
Type | dynamic write parameter |
Default | ClearWithProcessStart |
Range | {NoClearing, ClearWithProcessStart, ClearWithProcessReset, SendClearPulse} |
This parameter defines the reset behavior for all read parameters. NoClearing: Values of all read parameters are held. ProcessEnable and ProcessReset have no influcence on these values. ClearWithProcessStart: Values of read parameters are only cleared with rising edge of ProcessEnable. ClearWithProcessReset: Values of read parameters are only cleared with rising edge of ProcessReset. SendClearPulse: On-demand clearing of all read parameter values. |
MeasurementPeriod | |
---|---|
Type | dynamic read parameter |
Default | 1000 |
Range | [1, 65535] |
Time in milliseconds for rate and duty cycle measurements. . |
FrameCountWidth | |
---|---|
Type | static write parameter |
Default | 24 |
Range | [4, 63] |
Sets the bit width of the frame counter (parameter FrameCount). |
GapCountWidth | |
---|---|
Type | static write parameter |
Default | 20 |
Range | [4, 63] |
Sets the bit width of the line gap counters (MinLineGap, MaxLineGap, MeanLineGap, MinLinePeriod, MaxLinePeriod, MeanLinePeriod). |
FrameCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^FrameCountWidth) -1] |
Counts all images which are terminated with an EndOfFrame. Available only in IMAGE-2D mode. |
FramePixelCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^ (ImageWidthBitwidth+ImageHeightBitwidth+4))-1] |
Size of the last completed frame in pixels. |
MinWidth | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+4))-1] |
Minimal line width detected in all frames inspected so far (in pixels). |
MaxWidth | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+4))-1] |
Maximal line width detected in all frames inspected so far (in pixels). |
MinHeight | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageHeightBitwidth+4))-1] |
Minimal image height detected in all frames inspected so far (in pixels). |
MaxHeight | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageHeightBitwidth+4))-1] |
Maximal image height detected in all frames inspected so far (in pixels). |
MinPixelCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+ImageHeightBitwidth+4))-1] |
Size of smallest frame out of all frames inspected so far (in pixels). |
MaxPixelCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+ImageHeightBitwidth+4))-1] |
Size of biggest frame out of all frames inspected so far (in pixels). |
MinLineGap | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Minimal line gap encountered in all frames inspected so far. Does not include the frame gap between the last line of a 2D image and the first line of the next image. ![]() |
MaxLineGap | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Maximal line gap encountered encountered in all frames inspected so far. Does not include the frame gap between the last line of a 2D image and the first line of the next image. ![]() |
MinLinePeriod | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Minimal line period encountered. A Line period is the number of clock cycles between two line beginnings. A line period thus covers the line width, a single EndOfLine pulse, and the line gap. The frame gap between the last line of a 2D image and the first line of the next image is not included. ![]() |
MaxLinePeriod | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Maximal line period encountered. A Line period is the number of clock cycles between two line beginnings. A line period thus covers the line width, a single EndOfLine pulse, and the line gap. The frame gap between the last line of a 2D image and the first line of the next image is not included. ![]() |
MeanWidth | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+4))-1] |
Mean line width during set MeasurementPeriod (in pixels). |
MeanLinePeriod | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Mean line period during set MeasurementPeriod. A Line period is the number of clock cycles between two line beginnings. A line period thus covers the line width, a single EndOfLine pulse, and the line gap. The frame gap between the last line of a 2D image and the first line of the next image is not included. ![]() |
MeanLineGap | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^GapCountWidth)-1] |
Mean line gap during set MeasurementPeriod (mean number of clock cycles between two line beginnings). The frame gap between the last line of a 2D image and the first line of the next image is not included. ![]() |
MeanLineDutyCycle | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0.0, 100.0] |
Mean line duty cycle during set MeasurementPeriod. Defined as MeanWidth divided by MeanLinePeriod. ![]() |
LineRate | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | |
Line rate in Hertz. |
FrameRate | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | |
Frame rate in Hertz. |
BlockedFraction | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0.0, 100.0] |
Percentage of blocked cycles. |
IdleFraction | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0.0, 100.0] |
Percentage of idle cycles. |
ValidFraction | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0.0, 100.0] |
Percentage of valid cycles carrying data. |
MaxWidthErrorCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^(ImageWidthBitwidth+4))-1] |
Counts up if line width is greater than maximum line width defined on the input link. |
MaxHeightErrorCount | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, (2^( ImageHeightBitwidth+4))-1] |
Counts up if image height is greater than maximum image height defined on the input link. |
OverflowMask | |
---|---|
Type | dynamic read parameter |
Default | 0 |
Range | [0, 4095] |
Bit encoded overflow signaling. A set bit indicates an overflow in the following counters: [0] = FrameCount [1] = PixelCount [2] = xPos [3] = yPos [4] = LineGap [6] = MeanLineGap [8] = BlockedFraction [10] = ValidFraction [11] = LineCounter. Invalidates LineRate, MeanWidth, MeanLinePeriod and MeanLineGap. |
The use of operator ImageStatistics is shown in the following examples:
-
Example - For debugging purposes of the designs internal data flow control in hardware and a possible compensation.