Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Device Temperature (Stereo ace)#

The Device Temperature feature allows you to determine the camera temperature at its core board.

Monitoring the device temperature is important in order to make sure that the temperature state of the camera stays within the acceptable range.

Using the Feature#

Determining the Device Temperature#

To determine the device temperature:

  1. Select the camera whose temperature you want to measure using the BslCameraSelector parameter.
    The DeviceTemperatureSelector is set to Coreboard by default.
  2. Get the value of the DeviceTemperature parameter.

The temperature is given as a floating-point value in degrees Celsius.