Features#
You can configure the parameters via the Basler pylon API or via the Basler pylon Viewer.
Which Features Are Available for My Camera?#
To find out which features are available for a specific camera model:
- Select your camera model using the "Your camera model" filter at the top right corner of this page.
-
Check the entries in the "Features" section in the table of contents. The color of the entries indicates whether a feature is available:
(1) Feature is supported by the camera model currently selected.
(2) Feature is not supported by the camera model currently selected.