Intensity Calculation#
If you're capturing motion with blaze cameras, the setting of the IntensityCalculation parameter determines whether the depth map and the intensity image are in synch.
To specify the intensity calculation method:
- Set the
IntensityCalculationparameter to one of the following values:Method1: This is the default setting. In scenes containing motion you may notice a lag between depth map and intensity image.Method2: With this setting, the depth map and the intensity image are in synch but the resulting intensity image will be darker and contain more noise.