Pixel Format (Stereo ace)#
There are different pixel formats depending on the component selected.
Using the Feature#
Available Pixel Formats#
| Component Name | Pixel Format | Description |
|---|---|---|
| Intensity | Mono8RGB8 | Left rectified camera image |
| IntensityCombined | Mono8RGB8 | Left rectified camera image stacked on right rectified camera image |
| Disparity | Coord3D_C16 | Disparity image in desired resolution, i.e., depth resolution |
| Confidence | Confidence8 | Confidence image |
| Error | Error8 | Disparity error image |
The RGB8 format for intensity images is only available for color cameras.
Selecting a Pixel Format#
To select a pixel format for a component:
- Set the
ComponentSelectorparameter to the component for which you want to specify a pixel format. - Set the
ComponentEnableparameter totrueif it isn't enabled already. - Set the
PixelFormatparameter to the desired pixel format for the component. - Repeat for other components if required.