Stereo mini Features#
This section describes the features used to configure depth and color image acquisition on Stereo mini cameras.
You can configure the parameters via the pylon APIs included in the pylon Software Suite or via the 3D Viewer.
The available parameters, values, and value ranges can vary depending on the camera model, firmware version, selected source, and selected component. The 3D Viewer displays the settings available for the connected camera.
Selecting a Source#
Some image acquisition features are source-dependent. Before configuring one of these features, set the SourceSelector parameter to the sensor that you want to control:
Source1(Left): Left monochrome sensorSource2(Right): Right monochrome sensorSource3(Color): Color sensor
For information about the image streams, resolutions, and frame rates supported by each camera model, see Image Data Stream.