Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Using Stereo ace Cameras#

This topic gives a step-by-step overview over how to get started with Basler Stereo ace cameras. It will show you how to configure the camera, acquire images, and process the resulting image data.

The easiest way to work with Stereo ace cameras is via the Stereo Camera Viewer, which is installed as part of the pylon Supplementary Package for Stereo ace.

Step-By-Step Instructions#

  1. Connect the camera to your computer.
    For information about installing the camera and the software, see Hardware Installation (Stereo ace) and Software Installation (Stereo ace). When Status and Ethernet LEDs are flashing green / solid green, the camera is ready to use. For more information, see the "LED States" section of your camera model topic.
  2. Start the Stereo Camera Viewer.
    Windows: Click Start > Basler > Stereo Camera Viewer.
    Linux: Issue the following command: /opt/pylon/bin/StereoViewer
    The camera appears in the camera selector drop-down list and image acquisition starts immediately.
    In the image window area, four windows open that show the different components.
    If the camera is not shown in the camera selector, this may be due to problems with the IP address.
  3. Configure the camera. For more information about that, see Optimizing image quality (Stereo ace).
  4. Process the measurement results.
  5. Save the camera settings if desired.
    For more information about that, see Overview of the Stereo Camera Viewer.