White Balance#
Automatic White Balance#
To configure automatic white balance:
- Set the
SourceSelectorparameter toSource3(Color). - Set the
BalanceWhiteAutoparameter to one of the following values:Off: Automatic white balancing is disabled. Set the white balance manually using theBalanceRatioparameter.Continuous: The camera continuously adjusts the white balance while images are being acquired.
Manual White Balance#
To configure white balance manually:
- Set the
SourceSelectorparameter toSource3(Color). - Set the
BalanceWhiteAutoparameter toOff. - Set the
BalanceRatioparameter to the desired value.
The available range depends on the camera model and firmware version.