Blooming Reduction#
Using the Feature#
Enabling Blooming Reduction#
To enable blooming reduction:
- Make sure the camera is idle, i.e., not capturing images.
- Set the
BslBloomingReductionEnableparameter totrue.
Info
When the Blooming Reduction feature is enabled, the camera may set the Gain parameter to a higher value to avoid unwanted image effects.
Sample Code#
You can also use the pylon Viewer to easily set the parameters.