Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Configuring Basler GMSL Cameras#

This topic gives you information about setting up a GMSL system with Basler GMSL cameras and a host system. It guides you through the rough steps to be executed and gives you information about what to observe.

Before you start#

Make sure that the following steps have been executed and are available before starting the configuring procedure of the GMSL cameras:

Configuring GMSL Cameras#

The following sections show you how to configure one or multiple GMSL cameras:

Configuring a Single ace 2 GMSL Camera#

For a first view of the images in the pylon Viewer:

Info

If a camera is powered over the coax cable (PoC), it may be automatically switched off during shutdown and reboot.

  1. Make sure that the system components are powered (i.e., GMSL camera and host system (deserializer inclusive)).
  2. Start the pylon Viewer.
    The pylon Viewer automatically detects the connected cameras.
    During the camera enumeration, the camera supply is switched on. It may take a few seconds, depending on the host system, before the camera appears in the Devices pane.
  3. If the cameras are not automatically detected, click the Refresh icon to the right of the Auto-Scan check box.
  4. Double-click the desired camera in pylon Viewer.
    The device tree opens showing parameters for configuring the camera.

    pylon Viewer: Detecting the Camera

  5. To configure the parameters, enable the Show Tree View check box. Otherwise, the parameters are all listed in the same category.

  6. You can now acquire frames using the Continuous Shot acquisition mode pylon Viewer Continuous Shot Acquisition mode or the Single Shot acquisition mode pylon Viewer Single Shot Acquisition mode.
  7. Configure the camera with your custom settings as desired (e.g., define how you want to trigger (see Triggered Image Acquisition) and what Features you want to enable and configure).

Info

Depending on your host system, for each Basler ace 2 GMSL camera you can configure a number of link signals (i.e., virtual I/O signals). To find out how many link signals are available for your camera model, check the "General Specifications" table in your camera model topic. You can find your camera topic in the Area and Line Scan Cameras section.

Configuring Multiple ace 2 GMSL Cameras#

  1. Make sure that the system components are powered (i.e., GMSL cameras and host system (deserializer inclusive)).
  2. Execute steps 2. to 5. as described in the Configuring a Single ace 2 GMSL Camera section for all connected ace 2 GMSL cameras.

pylon Viewer with 4 ace 2 GMSL Cameras

  1. If you connected several GMSL cameras during the hardware installation, check the bandwidth settings via the Bandwidth Manager.
  2. If you want to optimize the bandwidth settings or change the bandwidth assignement, see the Optimizing Bandwidth Consumption section.

    • The available bandwidth depends on the hardware configuration and can vary between different host systems.
    • By default, the maximum possible bandwidth for each camera is assigned to the SoC via the CSI interface.
    • In many host systems, two or four GMSL ports are multiplexed to a single MIPI D-Phy interface, sharing its available data bandwidth. If you require another bandwidth assignment for your cameras, configure the bandwidth for each camera via the Bandwidth Manager.
    • You can save the adapted bandwidth values in a user set so that the camera wakes up with the stored settings after a restart (in pylon Viewer via the File Access command in the Camera menu).
  3. Continue with steps 6. to 8. as described in the Configuring a Single ace 2 GMSL Camera section.
    Execute the configuring steps for each GMSL camera you use in your system.

Info

If the bandwidth is not correctly set (e.g., the required bandwidth exceeds the available bandwidth), this can lead to incomplete images or images that are not displayed.

Bandwidth Manager with 2 ace 2 GMSL Cameras