Line Format#
Using the Feature#
Determining the Line Format#
To determine the electrical format of an I/O line:
- Set the
LineSelectorparameter to the desired I/O line, e.g.,Line1. - Get the value of the
LineFormatparameter.
This parameter is read-only.
Possible Values#
Possible values are:
NoConnect: The line is not connected.OptoCoupled: The line is an opto-coupled I/O line.OpenDrain,TTL,LVTTL, orRS422: The line is a general purpose I/O (GPIO) line.
Sample Code#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Select the desired I/O line */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line1");
CHECK(errRes);
/* Get the electrical format of the line */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "LineFormat", e_str, &len);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.