Sensor Readout Time#
Info
This feature only provides a very rough estimate of the sensor readout time. If you want to optimize the camera for triggered image acquisition or for overlapping image acquisition, use the Resulting Acquisition Frame Rate or Resulting Acquisition Line Rate feature instead.
Using the Feature#
Why Determine the Sensor Readout Time#
Each image acquisition process includes two parts:
- Exposure of the pixels of the image sensor, i.e., the exposure time.
- Readout of the pixel values from the sensor, i.e., the sensor readout time.
The Sensor Readout Time feature is useful if you want to estimate which part of the image acquisition process is limiting the camera's frame rate.
To do so, compare the exposure time with the sensor readout time:
- If the sensor readout time is considerably longer than the exposure time, consider adjusting camera features that affect the sensor readout time, e.g., Binning, Decimation, or Image ROI.
- If the sensor readout time is considerably shorter than the exposure time, consider reducing the exposure time.
Determining the Sensor Readout Time#
To determine the sensor readout time at the current settings, get the value of the SensorReadoutTime parameter. The sensor readout time is measured in microseconds.
The result is only an approximate value and depends on various camera settings and features, e.g., Binning, Decimation, or Image ROI.
Sample Code#
ace Classic/U/L GigE Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the sensor readout time at the current settings */
errRes = PylonDeviceGetFloatFeature(hdev, "ReadoutTimeAbs", &d);
CHECK(errRes);
Other Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the sensor readout time at the current settings */
errRes = PylonDeviceGetFloatFeature(hdev, "SensorReadoutTime", &d);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.