Basler Vision Connector Messaging: Deleting a Recipe Instance
This command deletes a recipe instance using the recipe instance ID specified when the recipe instance was created. You can delete the recipe instance even if cameras are currently assigned to the recipe pins.
JSON Payload
| Field | Optional | Type | Description |
| TransactionID | Yes | String | Transaction identification |
| Action | No | String | Method called. Fixed value: cstm_CloseRecipe |
| RecipeID | No | String | The user-defined ID that was used when instantiating the recipe. |
{
"TransactionID": "234423465465",
"Action": "cstm_CloseRecipe",
"RecipeID": "MyRecipeID"
}
Response Object
| Field | Optional | Type | Description |
| TransactionID | Yes | String | Transaction identification |
| ReturnCode | No | Integer | Message code following Message Codes |
| Message | No | String | Response message |
{
"TransactionID": "234423465465",
"ReturnCode": 0,
"Message": "Recipe closed."
}