Histogram Statistics vTool#
You can use the Histogram Extractor vTool to extract brightness values from an image and use those integer arrays as input.
Download the pylon Software Suite to use the Histogram Statistics vTool.

The vTool outputs the following statistical data:
- Minimum
- Maximum
- Mean
- Median
- StandardDeviation
- PixelCount
If you want to remove brightness values from the top and bottom of the distribution, e.g., because extremely high or low values may be caused by hot or dark pixels, you can do this via the following API parameters:
- Bottom Percentile: This allows you to specify which percentage of brightness values you want to remove from the bottom of the distribution. The default is 0.02, which means that values smaller than 2 percent of all values are removed.
- Top Percentile: This allows you to specify which percentage of brightness values you want to remove from the top of the distribution. The default is 0.02, which means that values higher than 98 percent of all values are removed.
- Discard: Enable this parameter to remove the top and bottom percentiles from the distribution before evaluation.
Configuring the vTool#
To configure the Histogram Statistics vTool, double-click it in the Workbench. A dialog opens showing all the available settings. Alternatively, you can find the same settings in the Features - All pane.
Inputs#
HistogramData#
Accepts integer arrays from the Histogram Extractor vTool.
- Data type: Image
Outputs#
Minimum#
Returns the lowest index position of the input array, i.e., brightness value, of the histogram.
- Data type: Float
Maximum#
Returns the highest index position of the input array, i.e., brightness value, of the histogram.
- Data type: Float
Mean#
Returns the mean value of the histogram.
- Data type: Float
Median#
Returns the median value of the histogram.
- Data type: Integer
StandardDeviation#
Returns the standard deviation of the histogram.
- Data type: Float
PixelCount#
Returns the overall number of pixels that contributed to the histogram.
- Data type: Integer