Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Basler Vision Connector Licensing#

To operate the Basler Vision Connector (BVC), the following licenses are required:

  • pylon License: Required to run the pylon software and create vTools in the pylon Viewer. The pylon license is included with the purchase of a Basler camera (see pylon EULA).
  • pylon vTools License: Required to create certain vTools in the pylon Viewer. A free trial license, valid for 180 days, is included with the pylon installation. You can find a list of vTools that require a license in the vTools Licenses section.
    For purchasing information, visit: pylon vTools Licenses.
  • Basler Vision Connector vTools Licenses: Required to instantiate certain vTools in the Basler Vision Connector. You can find a list of vTools that require a license in the vTools Licenses section.
    These licenses can be purchased through the Siemens Marketplace vTools Licenses.
  • Basler Vision Connector Multi-Camera Connection License: Required if you want to connect more than one camera simultaneously to the Basler Vision Connector.
    This license can be purchased through the Siemens Marketplace Multi-Camera Connection Licenses.
  • Siemens Industrial Edge Management License: Required to use the Siemens Industrial Edge Management System and to manage Siemens Industrial Edge Devices.
    For more information, see Siemens Xcelerator.

Info

The Basler Vision Connector app itself doesn't require a license. However, the BVC vTools licenses and the BVC Multi-Camera Connection License can be purchased in the Siemens Marketplace - BVC. vTools licenses can be purchased through the Siemens Marketplace - vTools.

vTools Licenses#

The following vTools require licenses: both a pylon vTools license and a Basler Vision Connector license are necessary.

Category vTool Name License Required
Acquisition Cameraa No
Image Loadinga No
Blob Analysis Absolute Thresholding Basic Yes
Auto Thresholding Basic Yes
Color Classifier Basic Yes
Region Feature Extraction Yes
Region Morphology Yes
Region Selection Yes
Relative Thresholding Basic Yes
Data Management Data Synchronizer No
Multiplexer No
Identification Barcode Reader Starter No
Barcode Reader Basic Yes
Barcode Reader Pro Yes
Data Matrix Code Reader Starter No
Data Matrix Code Reader Basic Yes
Data Matrix Code Reader Pro Yes
OCR Basic Yes
QR Code Reader Starter No
QR Code Reader Basic Yes
QR Code Reader Pro Yes
Image Manipulation Gray Value Transformer Starter No
Gray Value Transformer Basic Yes
Image Combiner Starter No
Image Combiner Basic Yes
Image Enhancer Basic Yes
Image Morphology Starter No
Image Morphology Basic Yes
Image Sharpening Starter No
Image Sharpening Basic Yes
Image Smoothing Starter No
Image Smoothing Basic Yes
Matching Geometric Pattern Matching Basic Yes
Geometric Pattern Matching Pro Yes
Template Matching Starter No
Template Matching Basic Yes
Measuring Circle Measurements Pro Yes
Ellipse Measurements Pro Yes
Line Measurements Pro Yes
Measurements Basic Yes
Rectangle Measurements Pro Yes
Supporters Array Element Selector No
Calibration Basic Yes
Calibration Pro Yes
Grid Creator No
Histogram Extractor No
Histogram Statistics No
Image Alignment No
Image Cropper No
Image Format Converter No
Image Stitcher No
Image Transformer No
Mini Script No
ROI Creator No
Region Combiner No

  1. Not supported by the Basler Vision Connector. If this vTool is included in the recipe file you want to instantiate in the Basler Vision Connector, it must be deactivated. See Using vTools in the Basler Vision Connector for details.

Assigning Licenses to Your Industrial Edge Device (IED)#

To use the Basler Vision Connector licenses (e.g., Basler Vision Connector vTools licenses and the Basler Vision Connector Multi-Camera Connection license), you must assign them to your Industrial Edge Device (IED).

For detailed instructions, refer to the official Siemens documentation: Managing Licenses: Siemens Industrial Edge.

Info

Basler recommends to assign licenses directly to Industrial Edge Devices, not to the Industrial Edge Management (IEM). This ensures that the correct licenses are reliably allocated to the correct devices.

When you assign one license (e.g., Basler Vision Connector vTools licenses and the Basler Vision Connector Multi-Camera Connection license) to an Edge Device, the device automatically claims all available BVC licenses assigned to its Edge Device or its Industrial Edge Management (IEM).

If you want to reassign a license to a different Edge Device, follow these steps:

  1. Stop the Basler Vision Connector on the current Edge Device.

    Stopping the Basler Vision Connector

  2. Wait for 2 hours.
    Reason: Licenses are reserved for the device for 2 hours after stopping the Basler Vision Connector.

  3. After 2 hours, change the license assignments in the Industrial Edge Hub.
  4. Restart the Vision Connector App on your Edge Device.

    Starting the Basler Vision Connector

You can stop and start the Basler Vision Connector either from the Industrial Edge Management (IEM) or via your Industrial Edge Device.