Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Integration with OpenCV#

This topic explains how to integrate pypylon image acquisition with OpenCV for visualization and image processing.

Why Use OpenCV?#

OpenCV is one of the most widely-used computer vision libraries. It provides the following features:

  • Fast image processing algorithms
  • Visualization tools
  • Support for feature detection, filtering, and analysis
  • Interoperability with NumPy

Since pypylon images are already NumPy arrays, integration is seamless.

Basic Workflow#

Camera → pypylon → NumPy Array → OpenCV → Display/Processing

Simple Example#

import cv2
from pypylon import pylon

with pylon.InstantCamera(pylon.FirstFound) as camera:
    camera.StartGrabbingMax(1)

    with camera.RetrieveResult(5000) as grab_result:
        if grab_result.GrabSucceeded():
            image = grab_result.Array

            # Display using OpenCV
            cv2.imshow("image", image)
            cv2.waitKey(0)
            cv2.destroyAllWindows()

Color Format Considerations#

OpenCV expects images in BGR format, while cameras may output the following formats:

  • Mono (grayscale)
  • Bayer
  • RGB

Converting Images to OpenCV-Compatible Formats#

For a live loop, prefer converter.ConvertToArray(grab_result): This writes the converted pixels directly into a pre-allocated NumPy array and avoids the extra copy of converter.Convert(grab_result).Array (see Working with Images for details).

converter = pylon.ImageFormatConverter()
converter.OutputPixelFormat = pylon.PixelType_BGR8packed
image = converter.ConvertToArray(grab_result)

Live Display Loop#

import cv2
from pypylon import pylon

with pylon.InstantCamera(pylon.FirstFound) as camera:
    camera.StartGrabbing(pylon.GrabStrategy_LatestImageOnly)

    while camera.IsGrabbing():
        with camera.RetrieveResult(5000) as grab_result:
            if grab_result.GrabSucceeded():
                image = grab_result.Array

                cv2.imshow("Live", image)

                if cv2.waitKey(1) == 27:  # ESC to exit
                    break

    cv2.destroyAllWindows()

Typical OpenCV Operations#

Grayscale Conversion#

gray = cv2.cvtColor(image, cv2.COLOR_BGR2GRAY)

Edge Detection#

edges = cv2.Canny(image, 50, 150)

Blur/Filtering#

blur = cv2.GaussianBlur(image, (5, 5), 0)

Drawing Overlays#

cv2.rectangle(image, (50, 50), (200, 200), (0, 255, 0), 2)

Combining NumPy and OpenCV#

This example demonstrates a complete vision pipeline combining pypylon, NumPy, and OpenCV. It continuously grabs images from the camera, extracts a fixed region of interest (ROI), computes a simple statistic (mean intensity), and visualizes the result directly in the live image.

These are the steps:

  1. An ROI is defined and extracted using NumPy slicing.
  2. The mean intensity of the ROI is calculated.
  3. The ROI is visualized using an OpenCV rectangle overlay.
  4. The result of a simple rule-based decision ("bright region") is displayed on the image.

This pattern represents a common real-world workflow:

Acquire → Select ROI → Compute Feature → Visualize → Decide
import cv2
from pypylon import pylon
import numpy as np

with pylon.InstantCamera(pylon.FirstFound) as camera:
    camera.StartGrabbing(pylon.GrabStrategy_LatestImageOnly)

    while camera.IsGrabbing():
        with camera.RetrieveResult(5000) as grab_result:
            if grab_result.GrabSucceeded():
                image = grab_result.Array

                # Define ROI coordinates
                y1, y2 = 100, 200
                x1, x2 = 200, 300

                # Extract ROI
                roi = image[y1:y2, x1:x2]

                # Compute statistics
                mean = np.mean(roi)

                # Draw rectangle around ROI
                cv2.rectangle(image, (x1, y1), (x2, y2), (0, 255, 0), 2)

                if mean > 100:
                    cv2.putText(image, "Bright Region", (50, 50),
                                cv2.FONT_HERSHEY_SIMPLEX, 1, (0, 255, 0), 2)

                cv2.imshow("Live", image)

                if cv2.waitKey(1) == 27:
                    break

    cv2.destroyAllWindows()

Key Takeaways#

  • pypylon integrates seamlessly with OpenCV via NumPy.
  • Color conversion is often required.
  • OpenCV provides powerful visualization and processing tools.
  • Combining NumPy and OpenCV enables flexible pipelines.