Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Working with Images#

This topic explains how image data is represented in pypylon, how to safely access it, and how to prepare it for further processing (e.g., with NumPy, OpenCV, or AI frameworks).

Image Representation#

In pypylon, images are exposed, e.g., as NumPy arrays, which means that they can be used directly in scientific and machine vision workflows.

This is a typical workflow:

Camera → GrabResult → Buffer → NumPy Array

Accessing Image Data#

It's essential to know when to copy the data from the grab result and when not to. Copying too much wastes time, while copying too little can lead to crashes or incorrect pixel data.

Code Description Copy Required?
.Array Returns a NumPy copy No (already a copy)
.GetMemoryView() Returns a buffer view Yes
.GetArrayZeroCopy() Returns a zero-copy array Yes
  • grab_result.Array is a copy of the internal buffer.
  • grab_result.GetMemoryView() is a view into an internal buffer (except for pixel types where pylon.IsPacked(grab_result.PixelType) is True).
  • grab_result.GetArrayZeroCopy() is a view into an internal buffer providing a NumPy array without copying (except for pixel types where pylon.IsPacked(grab_result.PixelType) is True).
  • The grab result buffer is released when leaving the with block or grab_result.Release() is called.
  • Accessing a memory view or zero-copy array after a buffer has been released can lead to invalid memory access.

Correct usage:

with camera.RetrieveResult(5000) as grab_result:
    if grab_result.GrabSucceeded():
        image = grab_result.Array

Image Shape and Format#

The shape of the array depends on the pixel format:

Pixel Format Shape Example
Mono8 (height, width)
RGB8/BGR8 (height, width, 3)

You can inspect the shape directly:

print(image.shape)

Pixel Format Conversion#

Depending on the camera configuration, the raw image format may not be suitable and may require conversion.

Example: Converting to BGR (OpenCV-compatible)

converter = pylon.ImageFormatConverter()
converter.OutputPixelFormat = pylon.PixelType_BGR8packed

image = converter.Convert(grab_result).GetArray()

Info

In ImageFormatConverter, OutputPixelFormat is a plain attribute that holds a pixel-type value, not a parameter node. Assign it directly (converter.OutputPixelFormat = pylon.PixelType_BGR8packed). It has no .Value accessor.

Converting Directly Into a NumPy Array (ConvertToArray)#

converter.Convert(src) returns a PylonImage. Reading its pixels with .Array (or .GetArray()), makes an additional copy of the converted buffer. If you only need the result as a NumPy array, use converter.ConvertToArray(src) instead. This pre-allocates a NumPy array with the correct shape and data type and lets the converter write the converted pixels directly into that array, avoiding the extra copy.

converter = pylon.ImageFormatConverter()
converter.OutputPixelFormat = pylon.PixelType_BGR8packed

# Equivalent result to converter.Convert(grab_result).Array, but without the extra copy.
image = converter.ConvertToArray(grab_result)

ConvertToArray accepts the same source types as Convert (a grab result, a PylonImage, a data component, or any IImage), and the resulting array's shape and data type reflect the OutputPixelFormat:

  • PixelType_Mono8 → (height, width), uint8
  • PixelType_Mono16 → (height, width), uint16
  • PixelType_RGB8packed / PixelType_BGR8packed → (height, width, 3), uint8

A bit-packed output format (one for which pylon.IsPacked(pixel_type) is True) has no unambiguous NumPy shape/data type, so ConvertToArray raises ValueError for it by default. Pass raw=True to obtain the converted bytes as a flat uint8 array instead:

# raw=True returns a flat uint8 array of the converted bytes,
# which is also how to handle bit-packed output formats.
raw_bytes = converter.ConvertToArray(grab_result, raw=True)
Approach Result Extra Copy?
converter.Convert(src).Array NumPy array via intermediate PylonImage Yes
converter.ConvertToArray(src) NumPy array written in place No
converter.ConvertToArray(src, raw=True) Flat uint8 array (also for packed formats) No

Why Conversion Is Necessary#

  • Cameras often output raw or Bayer formats.
  • Applications typically expect:
    • BGR (OpenCV)
    • RGB (visualization)

Common Pitfalls#

Using Data After Buffer Release#

with camera.RetrieveResult(...) as grab_result:
    image = grab_result.Array # NumPy array
    memory_view = grab_result.GetMemoryView()
    with grab_result.GetArrayZeroCopy() as zero_copy_array:
        ... process zero_copy_array (NumPy array) ...

This is unsafe because memory_view may now reference invalid memory. Always use result.Array if needed outside the block or keep the grab_result alive.

Ignoring the Pixel Format#

Always verify or explicitly set the pixel format. Ignoring this, may lead to the following consequences:

  • Wrong color interpretation
  • Incorrect processing results

Performance Overheads#

The following actions may reduce the performance:

  • Copying large images costs time
  • Conversion adds CPU load

Strategies to avoid this:

Using Images in Processing Pipelines#

Because images are NumPy arrays, they can be used directly with OpenCV, NumPy Operations, and AI/ML Frameworks.

This is a generalized illustration of an image pipeline.

Camera → GrabResult → NumPy Array → Processing → Output

This represents the central data flow of most computer vision systems.

OpenCV#

import cv2

cv2.imshow("image", image)
cv2.waitKey(1)

NumPy Operations#

mean = image.mean()

AI/ML Frameworks#

  • PyTorch
  • TensorFlow

Sample Image Processing Pipeline Using NumPy#

NumPy enables fast, vectorized image processing directly on acquired images.

The following sample is a small but realistic image processing pipeline using NumPy.

Sample Code#

import numpy as np
from pypylon import pylon

with pylon.InstantCamera(pylon.FirstFound) as camera:

    camera.StartGrabbingMax(100)

    while camera.IsGrabbing():
        with camera.RetrieveResult(5000) as grab_result:
            if grab_result.GrabSucceeded():
                image = grab_result.Array

                # Do something with the image data.

                if image.ndim == 3:
                    gray = image.mean(axis=2)
                else:
                    gray = image

                norm = gray / 255.0

                binary = norm > 0.5

                mean_intensity = norm.mean()
                bright_pixel_ratio = binary.mean()

                print(f"Mean intensity: {mean_intensity:.3f}")
                print(f"Bright pixels: {bright_pixel_ratio*100:.1f}%")

Here are some explanations of the individual steps:

  • Grayscale conversion:

    gray = image.mean(axis=2)
    
  • Normalization:

    norm = gray / 255.0
    
  • Thresholding:

    binary = norm > 0.5
    
  • Statistical evaluation:

    mean_intensity = norm.mean()
    bright_pixel_ratio = binary.mean()
    

A generalized NumPy image pipeline looks like this:

Raw Image → NumPy Array → Processing → Features → Decision

Key Takeaways#

  • Images are provided as NumPy arrays.
  • Always copy buffer data when needed.
  • Ensure you're using correct pixel formats.
  • Conversion may be required for downstream processing.