Payload Formats#
Info
Images and regions can occur in ZeroMQ and MQTT messages, but they only reference actual image or region data in ZeroMQ, because image and region data is very bulky and would therefore cause too much traffic for an MQTT broker. In MQTT messages, images and regions are only informative. If the actual image data/region data is required, use ZeroMQ.
MQTT:
- IE Common Payload Format, used to transfer data of recipes.
- Limited Recipe Payload Format without regions and images to transfer data of recipes.
ZeroMQ:
- Image Format
- Recipe Payload Format to transfer data of images and recipes.
You find detailed information about these payload formats in the following sections.