Skip to content

PLCamera.AcquisitionModeEnum Class#

Sets the image acquisition mode.

Applies to: CamEmu, CameraLink, GigE, Stereo ace, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

Visibility: Beginner

Selecting Parameters: AcquisitionAbort, AcquisitionStart, AcquisitionStop

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.AcquisitionModeEnum

Constructors#

 NameDescription
Public methodPLCamera.AcquisitionModeEnum Initializes a new instance of the PLCamera.AcquisitionModeEnum class
 

Properties#

 NameDescription
Public propertyContinuous

The acquisition mode is set to Continuous. The camera will acquire images until acquisition is stopped.

Applies to: CamEmu, CameraLink, GigE, Stereo ace, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

Public propertyMultiFrame

The acquisition mode is set to Multi Frame. The camera will acquire a number of images specified by the user.

Applies to: CameraLink, GigE and Stereo ace

Public propertyName The full name of AcquisitionMode (Overrides ParameterListEnum.Name.)
Public propertySingleFrame

The acquisition mode is set to Single Frame. The camera will acquire a single image.

Applies to: CamEmu, CameraLink, GigE, Stereo ace, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

 

Methods#

 NameDescription
Public methodToString The full name of AcquisitionMode (Overrides Object.ToString()()()().)
 

PLCamera.AcquisitionModeEnum.ToString Method#

The full name of AcquisitionMode

Return Value#

Type: String
Returns the full name of AcquisitionMode

PLCamera.AcquisitionModeEnum Constructor#

Initializes a new instance of the PLCamera.AcquisitionModeEnum class

PLCamera.AcquisitionModeEnum.Continuous Property#

The acquisition mode is set to Continuous. The camera will acquire images until acquisition is stopped.

Applies to: CamEmu, CameraLink, GigE, Stereo ace, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, blaze, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP

PLCamera.AcquisitionModeEnum.MultiFrame Property#

The acquisition mode is set to Multi Frame. The camera will acquire a number of images specified by the user.

Applies to: CameraLink, GigE and Stereo ace

PLCamera.AcquisitionModeEnum.Name Property#

The full name of AcquisitionMode

PLCamera.AcquisitionModeEnum.SingleFrame Property#

The acquisition mode is set to Single Frame. The camera will acquire a single image.

Applies to: CamEmu, CameraLink, GigE, Stereo ace, ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, boost V CoaXPress, dart 2 USB, dart USB, pulse USB and racer 2 CXP