PLCamera.AcquisitionStatusSelectorEnum Class#
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
Visibility: Expert
Selecting Parameters: AcquisitionStatus
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.AcquisitionStatusSelectorEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.AcquisitionStatusSelectorEnum | Initializes a new instance of the PLCamera.AcquisitionStatusSelectorEnum class |
Properties#
Name | Description | |
---|---|---|
AcquisitionActive | A check determines whether the camera is currently acquiring one or multiple frames. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
AcquisitionIdle | A check determines whether the camera is currently idle, i.e., not acquiring images. Applies to: GigE | |
AcquisitionTransfer | A check determines whether the camera is currently transferring an acquisition of one or multiple frames. Applies to: CameraLink and GigE | |
AcquisitionTriggerWait | A check determines whether the camera is currently waiting for a trigger to acquire one or multiple frames. Applies to: CameraLink and GigE | |
ExposureActive | A check determines whether the camera is currently exposing a frame. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
ExposureTriggerWait | A check determines whether the camera is currently waiting for an Exposure Start trigger signal. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameActive | A check determines whether the camera is currently capturing a frame. Applies to: CameraLink, GigE and ace USB | |
FrameBurstActive | A check determines whether the camera is currently doing a frame burst of one or many frames. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstTriggerActive | A check can be performed if the device is currently doing a frame burst of one or many frames. Applies to: ace USB | |
FrameBurstTriggerTransfer | A check can be performed if the device is currently transferring a frame burst of one or many frames. Applies to: ace USB | |
FrameBurstTriggerWait | A check determines whether the camera is currently waiting for a frame burst trigger. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
FrameTransfer | A check determines whether the camera is currently transferring a frame. Applies to: CameraLink, GigE and ace USB | |
FrameTriggerWait | A check determines whether the camera is currently waiting for a frame trigger. Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
LineTriggerWait | A check determines whether the camera is currently waiting for a line trigger. Applies to: CameraLink and GigE | |
Name | The full name of AcquisitionStatusSelector (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of AcquisitionStatusSelector (Overrides Object.ToString()()()().) |
PLCamera.AcquisitionStatusSelectorEnum.ToString Method#
The full name of AcquisitionStatusSelector
Return Value#
Type: String
Returns the full name of AcquisitionStatusSelector
PLCamera.AcquisitionStatusSelectorEnum Constructor#
Initializes a new instance of the PLCamera.AcquisitionStatusSelectorEnum class
PLCamera.AcquisitionStatusSelectorEnum.AcquisitionActive Property#
A check determines whether the camera is currently acquiring one or multiple frames.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.AcquisitionIdle Property#
A check determines whether the camera is currently idle, i.e., not acquiring images.
Applies to: GigE
PLCamera.AcquisitionStatusSelectorEnum.AcquisitionTransfer Property#
A check determines whether the camera is currently transferring an acquisition of one or multiple frames.
Applies to: CameraLink and GigE
PLCamera.AcquisitionStatusSelectorEnum.AcquisitionTriggerWait Property#
A check determines whether the camera is currently waiting for a trigger to acquire one or multiple frames.
Applies to: CameraLink and GigE
PLCamera.AcquisitionStatusSelectorEnum.ExposureActive Property#
A check determines whether the camera is currently exposing a frame.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.ExposureTriggerWait Property#
A check determines whether the camera is currently waiting for an Exposure Start trigger signal.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.FrameActive Property#
A check determines whether the camera is currently capturing a frame.
Applies to: CameraLink, GigE and ace USB
PLCamera.AcquisitionStatusSelectorEnum.FrameBurstActive Property#
A check determines whether the camera is currently doing a frame burst of one or many frames.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.FrameBurstTriggerActive Property#
A check can be performed if the device is currently doing a frame burst of one or many frames.
Applies to: ace USB
PLCamera.AcquisitionStatusSelectorEnum.FrameBurstTriggerTransfer Property#
A check can be performed if the device is currently transferring a frame burst of one or many frames.
Applies to: ace USB
PLCamera.AcquisitionStatusSelectorEnum.FrameBurstTriggerWait Property#
A check determines whether the camera is currently waiting for a frame burst trigger.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.FrameTransfer Property#
A check determines whether the camera is currently transferring a frame.
Applies to: CameraLink, GigE and ace USB
PLCamera.AcquisitionStatusSelectorEnum.FrameTriggerWait Property#
A check determines whether the camera is currently waiting for a frame trigger.
Applies to: CamEmu, CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.AcquisitionStatusSelectorEnum.LineTriggerWait Property#
A check determines whether the camera is currently waiting for a line trigger.
Applies to: CameraLink and GigE
PLCamera.AcquisitionStatusSelectorEnum.Name Property#
The full name of AcquisitionStatusSelector