Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.BslFlatFieldCorrectionSelectorEnum Class#

Sets which type of flat-field correction can be configured.

Applies to: ace 2 GigE

Visibility: Beginner

Selecting Parameters: BslFlatFieldCorrectionMode, BslFlatFieldCorrectionSetIndex, BslFlatFieldCorrectionSetStatus

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslFlatFieldCorrectionSelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.BslFlatFieldCorrectionSelectorEnum Initializes a new instance of the PLCamera.BslFlatFieldCorrectionSelectorEnum class
 

Properties#

 NameDescription
Public propertyBlockBased

Block-based flat-field correction is performed.

Applies to: ace 2 GigE

Public propertyName The full name of BslFlatFieldCorrectionSelector (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of BslFlatFieldCorrectionSelector (Overrides Object.ToString()()()().)
 

PLCamera.BslFlatFieldCorrectionSelectorEnum.ToString Method#

The full name of BslFlatFieldCorrectionSelector

Return Value#

Type: String
Returns the full name of BslFlatFieldCorrectionSelector

PLCamera.BslFlatFieldCorrectionSelectorEnum Constructor#

Initializes a new instance of the PLCamera.BslFlatFieldCorrectionSelectorEnum class

PLCamera.BslFlatFieldCorrectionSelectorEnum.BlockBased Property#

Block-based flat-field correction is performed.

Applies to: ace 2 GigE

PLCamera.BslFlatFieldCorrectionSelectorEnum.Name Property#

The full name of BslFlatFieldCorrectionSelector