PLCamera.BslFrequencyConverterActivationEnum Class#
Applies to: racer 2 CXP
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslFrequencyConverterActivationEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslFrequencyConverterActivationEnum | Initializes a new instance of the PLCamera.BslFrequencyConverterActivationEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | AnyEdge | An input pulse is triggered when the source signal falls or rises. Applies to: racer 2 CXP |
![]() | FallingEdge | An input pulse is triggered when the source signal falls. Applies to: racer 2 CXP |
![]() | Name | The full name of BslFrequencyConverterActivation (Overrides ParameterListEnum.Name.) |
![]() | RisingEdge | An input pulse is triggered when the source signal rises. Applies to: racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslFrequencyConverterActivation (Overrides Object.ToString()()()().) |
PLCamera.BslFrequencyConverterActivationEnum.ToString Method#
The full name of BslFrequencyConverterActivation
Return Value#
Type: String
Returns the full name of BslFrequencyConverterActivation
PLCamera.BslFrequencyConverterActivationEnum Constructor#
Initializes a new instance of the PLCamera.BslFrequencyConverterActivationEnum class
PLCamera.BslFrequencyConverterActivationEnum.AnyEdge Property#
An input pulse is triggered when the source signal falls or rises.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterActivationEnum.FallingEdge Property#
An input pulse is triggered when the source signal falls.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterActivationEnum.Name Property#
The full name of BslFrequencyConverterActivation
PLCamera.BslFrequencyConverterActivationEnum.RisingEdge Property#
An input pulse is triggered when the source signal rises.
Applies to: racer 2 CXP