PLCamera.BslLightDeviceChangeIDEnum Class#
Applies to: GigE and ace USB
Visibility: Expert
Selected by: BslLightDeviceSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightDeviceChangeIDEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslLightDeviceChangeIDEnum | Initializes a new instance of the PLCamera.BslLightDeviceChangeIDEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Device1 | The ID of the currently selected light device is changed to Device 1. Applies to: GigE and ace USB |
![]() | Device2 | The ID of the currently selected light device is changed to Device 2. Applies to: GigE and ace USB |
![]() | Device3 | The ID of the currently selected light device is changed to Device 3. Applies to: GigE and ace USB |
![]() | Device4 | The ID of the currently selected light device is changed to Device 4. Applies to: GigE and ace USB |
![]() | Name | The full name of BslLightDeviceChangeID (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslLightDeviceChangeID (Overrides Object.ToString()()()().) |
PLCamera.BslLightDeviceChangeIDEnum.ToString Method#
The full name of BslLightDeviceChangeID
Return Value#
Type: String
Returns the full name of BslLightDeviceChangeID
PLCamera.BslLightDeviceChangeIDEnum Constructor#
Initializes a new instance of the PLCamera.BslLightDeviceChangeIDEnum class
PLCamera.BslLightDeviceChangeIDEnum.Device1 Property#
The ID of the currently selected light device is changed to Device 1.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device2 Property#
The ID of the currently selected light device is changed to Device 2.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device3 Property#
The ID of the currently selected light device is changed to Device 3.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Device4 Property#
The ID of the currently selected light device is changed to Device 4.
Applies to: GigE and ace USB
PLCamera.BslLightDeviceChangeIDEnum.Name Property#
The full name of BslLightDeviceChangeID