PLCamera.BslLightDeviceNewIDEnum Class#
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslLightDeviceNewIDEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslLightDeviceNewIDEnum | Initializes a new instance of the PLCamera.BslLightDeviceNewIDEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Device1 | The ID of the currently selected light device can be set to Device 1. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Device2 | The ID of the currently selected light device can be set to Device 2. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Device3 | The ID of the currently selected light device can be set to Device 3. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Device4 | The ID of the currently selected light device can be set to Device 4. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Name | The full name of BslLightDeviceNewID (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslLightDeviceNewID (Overrides Object.ToString()()()().) |
PLCamera.BslLightDeviceNewIDEnum.ToString Method#
The full name of BslLightDeviceNewID
Return Value#
Type: String
Returns the full name of BslLightDeviceNewID
PLCamera.BslLightDeviceNewIDEnum Constructor#
Initializes a new instance of the PLCamera.BslLightDeviceNewIDEnum class
PLCamera.BslLightDeviceNewIDEnum.Device1 Property#
The ID of the currently selected light device can be set to Device 1.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslLightDeviceNewIDEnum.Device2 Property#
The ID of the currently selected light device can be set to Device 2.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslLightDeviceNewIDEnum.Device3 Property#
The ID of the currently selected light device can be set to Device 3.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslLightDeviceNewIDEnum.Device4 Property#
The ID of the currently selected light device can be set to Device 4.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.BslLightDeviceNewIDEnum.Name Property#
The full name of BslLightDeviceNewID