PLCamera.BslSensorAcquisitionModeEnum Class#
Applies to: racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslSensorAcquisitionModeEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.BslSensorAcquisitionModeEnum | Initializes a new instance of the PLCamera.BslSensorAcquisitionModeEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | DualLine | The sensor acquisition mode is set to Dual Line. Applies to: racer 2 CXP |
![]() | Name | The full name of BslSensorAcquisitionMode (Overrides ParameterListEnum.Name.) |
![]() | QuadLine | The sensor acquisition mode is set to Quad Line. Applies to: racer 2 CXP |
![]() | SingleLine | The sensor acquisition mode is set to Single Line. Applies to: racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of BslSensorAcquisitionMode (Overrides Object.ToString()()()().) |
PLCamera.BslSensorAcquisitionModeEnum.ToString Method#
The full name of BslSensorAcquisitionMode
Return Value#
Type: String
Returns the full name of BslSensorAcquisitionMode
PLCamera.BslSensorAcquisitionModeEnum Constructor#
Initializes a new instance of the PLCamera.BslSensorAcquisitionModeEnum class
PLCamera.BslSensorAcquisitionModeEnum.DualLine Property#
The sensor acquisition mode is set to Dual Line.
Applies to: racer 2 CXP
PLCamera.BslSensorAcquisitionModeEnum.Name Property#
The full name of BslSensorAcquisitionMode
PLCamera.BslSensorAcquisitionModeEnum.QuadLine Property#
The sensor acquisition mode is set to Quad Line.
Applies to: racer 2 CXP
PLCamera.BslSensorAcquisitionModeEnum.SingleLine Property#
The sensor acquisition mode is set to Single Line.
Applies to: racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE