PLCamera.BslShadingCorrectionSetCreateStatusEnum Class#
Applies to: racer 2 CXP
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslShadingCorrectionSetCreateStatusEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslShadingCorrectionSetCreateStatusEnum | Initializes a new instance of the PLCamera.BslShadingCorrectionSetCreateStatusEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Active | A shading correction set is being created. Applies to: racer 2 CXP |
![]() | ErrorReverseX | A Reverse X error occurred while creating a shading correction set. A shading correction set can only be created when Reverse X is disabled. Applies to: racer 2 CXP |
![]() | Inactive | No shading correction set is being created. Applies to: racer 2 CXP |
![]() | Name | The full name of BslShadingCorrectionSetCreateStatus (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslShadingCorrectionSetCreateStatus (Overrides Object.ToString()()()().) |
PLCamera.BslShadingCorrectionSetCreateStatusEnum.ToString Method#
The full name of BslShadingCorrectionSetCreateStatus
Return Value#
Type: String
Returns the full name of BslShadingCorrectionSetCreateStatus
PLCamera.BslShadingCorrectionSetCreateStatusEnum Constructor#
Initializes a new instance of the PLCamera.BslShadingCorrectionSetCreateStatusEnum class
PLCamera.BslShadingCorrectionSetCreateStatusEnum.Active Property#
A shading correction set is being created.
Applies to: racer 2 CXP
PLCamera.BslShadingCorrectionSetCreateStatusEnum.ErrorReverseX Property#
A Reverse X error occurred while creating a shading correction set. A shading correction set can only be created when Reverse X is disabled.
Applies to: racer 2 CXP
PLCamera.BslShadingCorrectionSetCreateStatusEnum.Inactive Property#
No shading correction set is being created.
Applies to: racer 2 CXP
PLCamera.BslShadingCorrectionSetCreateStatusEnum.Name Property#
The full name of BslShadingCorrectionSetCreateStatus