PLCamera.BslTDINumberOfStagesEnum Class#
Applies to: racer 2 COF
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslTDINumberOfStagesEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.BslTDINumberOfStagesEnum | Initializes a new instance of the PLCamera.BslTDINumberOfStagesEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of BslTDINumberOfStages (Overrides ParameterListEnum.Name.) |
![]() | Stages128 | 128 Stages. Applies to: racer 2 COF |
![]() | Stages192 | 192 Stages. Applies to: racer 2 COF |
![]() | Stages224 | 224 Stages. Applies to: racer 2 COF |
![]() | Stages252 | 252 Stages. Applies to: racer 2 COF |
![]() | Stages256 | 256 Stages. Applies to: racer 2 COF |
![]() | Stages32 | 32 Stages. Applies to: racer 2 COF |
![]() | Stages4 | 4 Stages. Applies to: racer 2 COF |
![]() | Stages64 | 64 Stages. Applies to: racer 2 COF |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of BslTDINumberOfStages (Overrides Object.ToString()()()().) |
PLCamera.BslTDINumberOfStagesEnum.ToString Method#
The full name of BslTDINumberOfStages
Return Value#
Type: String
Returns the full name of BslTDINumberOfStages
PLCamera.BslTDINumberOfStagesEnum Constructor#
Initializes a new instance of the PLCamera.BslTDINumberOfStagesEnum class
PLCamera.BslTDINumberOfStagesEnum.Name Property#
The full name of BslTDINumberOfStages
PLCamera.BslTDINumberOfStagesEnum.Stages128 Property#
128 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages192 Property#
192 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages224 Property#
224 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages252 Property#
252 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages256 Property#
256 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages32 Property#
32 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages4 Property#
4 Stages.
Applies to: racer 2 COF
PLCamera.BslTDINumberOfStagesEnum.Stages64 Property#
64 Stages.
Applies to: racer 2 COF