PLCamera.CxpLinkConfigurationPreferredEnum Class#
Applies to: boost CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpLinkConfigurationPreferredEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.CxpLinkConfigurationPreferredEnum | Initializes a new instance of the PLCamera.CxpLinkConfigurationPreferredEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Auto | The link configuration is set to automatic discovery. Applies to: boost CoaXPress |
![]() | CXP10_X1 | The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps). Applies to: boost CoaXPress |
![]() | CXP10_X2 | The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps). Applies to: boost CoaXPress |
![]() | CXP12_X1 | The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps). Applies to: boost CoaXPress |
![]() | CXP12_X2 | The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps). Applies to: boost CoaXPress |
![]() | CXP2_X1 | The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps). Applies to: boost CoaXPress |
![]() | CXP2_X2 | The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps). Applies to: boost CoaXPress |
![]() | CXP3_X1 | The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps). Applies to: boost CoaXPress |
![]() | CXP3_X2 | The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps). Applies to: boost CoaXPress |
![]() | CXP5_X1 | The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps). Applies to: boost CoaXPress |
![]() | CXP5_X2 | The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps). Applies to: boost CoaXPress |
![]() | CXP6_X1 | The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps). Applies to: boost CoaXPress |
![]() | CXP6_X2 | The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps). Applies to: boost CoaXPress |
![]() | Name | The full name of CxpLinkConfigurationPreferred (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of CxpLinkConfigurationPreferred (Overrides Object.ToString()()()().) |
PLCamera.CxpLinkConfigurationPreferredEnum.ToString Method#
The full name of CxpLinkConfigurationPreferred
Return Value#
Type: String
Returns the full name of CxpLinkConfigurationPreferred
PLCamera.CxpLinkConfigurationPreferredEnum Constructor#
Initializes a new instance of the PLCamera.CxpLinkConfigurationPreferredEnum class
PLCamera.CxpLinkConfigurationPreferredEnum.Auto Property#
The link configuration is set to automatic discovery.
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP10_X1 Property#
The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP10_X2 Property#
The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP12_X1 Property#
The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP12_X2 Property#
The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP2_X1 Property#
The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP2_X2 Property#
The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP3_X1 Property#
The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP3_X2 Property#
The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP5_X1 Property#
The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP5_X2 Property#
The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP6_X1 Property#
The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.CXP6_X2 Property#
The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps).
Applies to: boost CoaXPress
PLCamera.CxpLinkConfigurationPreferredEnum.Name Property#
The full name of CxpLinkConfigurationPreferred