PLCamera.TimerSequenceEntrySelectorEnum Class#
Visibility: Guru
Selecting Parameters: TimerSequenceTimerSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TimerSequenceEntrySelectorEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.TimerSequenceEntrySelectorEnum | Initializes a new instance of the PLCamera.TimerSequenceEntrySelectorEnum class |
Properties#
Methods#
Name | Description | |
---|---|---|
ToString | The full name of TimerSequenceEntrySelector (Overrides Object.ToString()()()().) |
PLCamera.TimerSequenceEntrySelectorEnum.ToString Method#
The full name of TimerSequenceEntrySelector
Return Value#
Type: String
Returns the full name of TimerSequenceEntrySelector
PLCamera.TimerSequenceEntrySelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSequenceEntrySelectorEnum class
PLCamera.TimerSequenceEntrySelectorEnum.Entry1 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry10 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry11 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry12 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry13 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry14 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry15 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry16 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry2 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry3 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry4 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry5 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry6 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry7 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry8 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Entry9 Property#
PLCamera.TimerSequenceEntrySelectorEnum.Name Property#
The full name of TimerSequenceEntrySelector