PLTransportLayer Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.PLTransportLayer
Properties#
Name | Description | |
---|---|---|
![]() ![]() | AreaTriggerMode | Sets the trigger mode of the area trigger signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | AutomaticFormatControl | Enables/disables automatic control of the pixel format in the device. If enabled, the frame grabber's pixel format and its dependencies are automatically updated to match the camera's pixel format setting. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | AutomaticROIControl | Activates or deactivates the automatic control of the ROI in the Device. If this feature is active, the frame grabber ROI is automatically updated to the camera one. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | BitAlignment | Sets the alignment of the bits in the output format. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | CommandDuplicationEnable | Enables sending all commands and receiving all acknowledges twice. This option should only be enabled in case of network problems. Applies to: GigE and blaze Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | ConnectionGuardEnable | Enables the automatic start of the PylonGigEConnectionGuard. Applies to: GigE Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | CorrectedErrorCount | Number of errors corrected. This parameter indicates single-byte error correction in CXP stream packets. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | CustomBitShiftRight | User-defined bit shift to the right. This allows you to shift the pixel data in the output format to the right by a value of your choice. The Alignment parameter has to be set to CustomBitShift for this. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | CxpLinkConfiguration | Sets the link configuration for the communication between the receiver and transmitter device. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | CxpTriggerPacketMode | Sets the trigger packet mode. This parameter allows you to send triggers on rising edges only. It can be used for extreme trigger rates. This parameter may violate the CXP standard. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceAccessStatus | Returns the device's access status at the moment when the Device Update List command was last executed. This value only changes when the Device Update List command is executed. Applies to: CoaXPress and blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceDisplayName | User-friendly name of the device. Applies to: CoaXPress and blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceEndianessMechanism | Sets the endianness handling mode. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceID | Interface-wide unique ID of the selected device. This value only changes when the Device Update List command is executed. Applies to: CoaXPress and blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceManufacturerInfo | Additional information about the manufacturer of the device. Applies to: blaze Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | DeviceModelName | Name of the device model. This value only changes when the Device Update List command is executed. Applies to: CoaXPress and blaze Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | DeviceSerialNumber | Serial number of the remote device. This value only changes when the Device Update List command is executed. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceType | Returns the transport layer of the device. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | DeviceVendorName | Name of the device vendor. This value only changes when the Device Update List command is executed. Applies to: CoaXPress and blaze Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | EventDeviceLost | Returns the unique Identifier of the Device Lost event. Applies to: CoaXPress and blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | EventNotification | Sets whether the host application is notified of the selected event. Applies to: CoaXPress and blaze Visibility: Expert Selected by: EventSelector The feature documentation may provide more information. |
![]() ![]() | EventSelector | Sets which event to signal to the host application. Applies to: CoaXPress and blaze Visibility: Expert Selecting Parameters: EventNotification The feature documentation may provide more information. |
![]() ![]() | FillLevel | Current buffer fill level. This value allows you to check whether the average input bandwidth of the camera is too high to be processed by the applet. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Format | Sets the pixel format of the image that is output to the computer. The data is converted from the internal bit width and color format to the output format selected. This setting is not related to the pixel format input from the camera sensor. For more information, see the Pixel Format parameter documentation. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | FrontGPI | Current input signal levels of all front GPI inputs (bit mask). Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | GentlInfoIgnorefgformat | Ignore the FG output format and manage it internally in the GenTL producer Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | GentlInfoVersion | Version of the GenTL description Interface in the applet. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | GevDeviceGateway | Current gateway IP address of the GVCP interface of the remote device. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | GevDeviceIPAddress | Current IP address of the GVCP interface of the remote device. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | GevDeviceMACAddress | 48-bit MAC address of the GVCP interface of the remote device. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | GevDeviceSubnetMask | Current subnet mask of the GVCP interface of the remote device. Applies to: blaze Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | GPI | Current input signal levels of all GPI inputs (Bitmask). Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | HeartbeatTimeout | Heartbeat timeout value on the host side in milliseconds. This parameter is linked with the Heartbeat Timeout camera parameter. If the camera parameter changes, the host parameter changes accordingly, and vice versa. Applies to: GigE Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | Height | Height of the image ROI on the host side. This parameter is linked with the Height camera parameter. If the camera parameter changes, the host parameter changes accordingly, but not vice versa. The host parameter should not be set to a value different from the camera parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ImageSelect | Defines which image in a sequence is grabbed. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ImageSelectPeriod | Select the length of an image sequence. Only a single image of the sequence is grabbed. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LinkCommandRetryCount | Specifies maximum number of tries before failing the control channel commands. Applies to: blaze Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | LinkCommandTimeout | Specifies application timeout for the control channel communication. Up to DeviceLinkCommandRetryCount attempts with this timeout are made before a command fails with a timeout error. Applies to: blaze Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | LutCustomFile | Filename with custom lookup table values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutEnable | Switch the LUT and processing functionality on or off. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutImplementationType | Type of LUT implementation. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutInputPixelBitDepth | Pixel bit depth at LUT input. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutOutputPixelBitDepth | Pixel bit depth at LUT output. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutSaveFile | Save current LUT configuration. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutType | Enables the LUT to be loaded with custom values or uses the applet's processor. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValue | Field with LUT Values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueBlue | Field with blue LUT Values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueBlueSelector | Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueGreen | Field with green LUT Values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueGreenSelector | Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueRed | Field with red LUT Values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueRedSelector | Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | LutValueSelector | Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | MaxRetryCountRead | Maximum number of retries for read operations after a read operation has timed out. Applies to: GigE Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | MaxRetryCountWrite | Maximum number of retries for write operations after a write operation has timed out. Applies to: GigE Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | MigrationModeEnable | Enables mapping of certain SFNC 1.x node names to SFNC 2.x node names. This allows you to write code for camera devices that are compatible with different SFNC (Standard Features Naming Convention) versions. Available for USB camera devices only. Applies to: GigE and USB Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | MissingCameraFrameResponse | Returns whether missing frames are reported. If no frame is received for a trigger pulse, the parameter is set to Yes. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | MissingCameraFrameResponseClear | Clears the Missing Camera Frame Response parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | OffsetX | X-offset of the acquisition ROI independent of the camera ROI. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | OffsetY | Y-offset of the acquisition ROI independent of the camera ROI. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | OutputPackedFormats | Automatically outputs packed formats instead of unpacked ones. This parameter is only available if the Automatic Format Control parameter is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Overflow | Indicates whether if the image buffer is currently in overflow state. An overflow results in the loss of images. The parameter is reset at each readout cycle. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | PacketTagErrorCount | Number of packet errors. This parameter indicates that CXP stream packets are lost. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | PixelDepth | Applet-internal processing bit depth. This is the maximum bit depth at which pixels are processed. If you select a highter output and input bit depth, data may be truncated. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | PixelFormat | Sets the format of the pixel data transmitted by the camera. This setting has to match the pixel format set in the camera. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ProcessingGain | Gain correction value. Available when LUT functionality is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ProcessingGamma | Gamma correction value. Available when LUT functionality is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ProcessingInvert | Invert output. Available when LUT functionality is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ProcessingOffset | Offset correction value. Available when LUT functionality is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ReadTimeout | Read access timeout value in milliseconds. Applies to: GigE Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | ScalingFactorBlue | Blue gain of the white balancing. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ScalingFactorGreen | Green gain of the white balancing. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | ScalingFactorRed | Red gain of the white balancing. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SendSoftwareTrigger | Sends a software trigger pulse or adds pulses to the trigger queue if it is enabled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SensorHeight | Sensor Height in selected tap geometry. Value is ignored if vantage point = TopLeft. Available DRAM and SensorWidth limit the maximum SensorHeight. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SensorWidth | Sensor width in selected tap geometry. Value is ignored if vantage point = Top-Left. Available DRAM and SensorHeight limit the maximum SensorWidth. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SoftwareTriggerIsBusy | Indicates whether the software trigger is busy. This allows you to find out whether the trigger system is still processing software trigger pulses. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SoftwareTriggerQueueFillLevel | Number of pulses in queue to be processed. The Queue parameter needs to be enabled for this. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Last_Error_Status | Last error status of a read or write operation. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Last_Error_Status_Text | Last error status of a read or write operation. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Read_Operations_Failed_Count | Number of failed read operations. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Read_Pipe_Reset_Count | Number of read pipe resets. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Write_Operations_Failed_Count | Number of failed write operations. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Statistic_Write_Pipe_Reset_Count | Number of write pipe resets. Applies to: USB Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | StatisticReadWriteTimeoutCount | Number of timeouts during read and write operations when waiting for a response from the device. Applies to: GigE and blaze Visibility: Guru The feature documentation may provide more information. |
![]() ![]() | StreamDisplayName | User-friendly name of the selected stream. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | StreamID | Device-wide unique ID of the data stream. Applies to: CoaXPress and blaze Visibility: Beginner Selected by: StreamSelector The feature documentation may provide more information. |
![]() ![]() | StreamSelector | Sets the stream channel. The parameter is 0-based in order to match the index of the C interface. Applies to: CoaXPress and blaze Visibility: Beginner Selecting Parameters: StreamID The feature documentation may provide more information. |
![]() ![]() | SystemmonitorByteAlignment8b10bLocked | Byte Alignment 8b10b locked Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorChannelCurrent | Returns the Channel Current. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorChannelCurrentSelector | Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorChannelVoltage | Returns the Channel Voltage. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorChannelVoltageSelector | Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorCurrentLinkSpeed | Returns the current PCIe link speed in Gibibyte (2^30 byte). Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorCxpImageLineMode | This parameter informs on the current transfer mode, used by the camera. The transfer can be an areascan (= 0) or linescan (= 1) image. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SystemmonitorDisparity8b10bError | Disparity 8b 10b errors Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorExternalPower | Shows the external power state of the board. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorFpgaTemperature | Returns the current FPGA die temperature. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorFpgaVccAux | Returns the current FPGA auxiliary Vcc. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorFpgaVccBram | Returns the current FPGA BRAM Vcc. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorFpgaVccInt | Returns the current FPGA internal Vcc. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorNotInTable8b10bError | Not in table 8b 10b errors Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPacketbufferOverflowCount | Represents the number of overflows, if an overflow occurred due to not correctly aligned package order. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPacketbufferOverflowSource | Represents the port, which has overflows due to not correctly aligned package order. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPcieTrainedPayloadSize | Returns the PCIe trained payload size. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPcieTrainedRequestSize | Returns the PCIe trained request size. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPortBitRate | Returns the port bit rate Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorPowerOverCxpState | Shows the current power over CXP state. Applies to: CoaXPress Visibility: Beginner The feature documentation may provide more information. |
![]() ![]() | SystemmonitorUsedCxpConnections | The currently used number of CXP ports used in this process. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerAcknowledgementCount | Number of trigger acknowledgement packets sent by the camera (in response to trigger edge packets sent before) have been received by the frame grabber. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerCameraOutSelect | Sets the output source to be connected to a camera signal channel. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerEventCount | Number of trigger events sent to the camera. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerExceededPeriodLimits | Returns whether the input signal frequency exceeded the maximum specified. If the parameter returns Yes, signals were dropped. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerExceededPeriodLimitsClear | Clears the Trigger Exceeded Period Limits parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInDebounce | Input debounce time for trigger input signals (in microseconds). This parameter allows you to filter out invalid signals by specifying a minimum signal length. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInDownscale | Factor by which the trigger input signal is downscaled. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInDownscalePhase | Phase for selecting the desired pulse in the sequence. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInPolarity | Sets the polarity of the trigger input signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInSource | Sets the trigger input source for external trigger mode. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsFrequency | Current frequency of the input pulses. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsMaximumFrequency | Maximum input frequency detected. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsMinimumFrequency | Minimum input frequency detected. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsMinMaxFrequencyClear | Clears the minimum and maximum frequency values. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsPolarity | Sets the polarity of the trigger input signal for statistics. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsPulseCount | Number of input pulses. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsPulseCountClear | Clears the input signal pulse counter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerInStatisticsSource | Sets the trigger input source for statistics. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerMultiplyPulses | Upscales, i.e., duplicates, the number of trigger pulses generated externally or via software with the period specified by the Trigger Output Frequency parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutputFrequency | Maximum trigger output frequency. If the internal generator is used, it will use the frequency specified there. If an external source is used, this value determines the maximum allowed value. External trigger signals exceeding this value will be discarded. For more information, see the applet documentation. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectFrontGPO0 | Sets the output source of Front GPO 0. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectFrontGPO1 | Sets the output source of Front GPO 1. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO0 | Sets the output source of GPO 0. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO1 | Sets the output source of GPO 1. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO2 | Sets the output source of GPO 2. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO3 | Sets the output source of GPO 3. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO4 | Sets the output source of GPO 4. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO5 | Sets the output source of GPO 5. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO6 | Sets the output source of GPO 6. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutSelectGPO7 | Sets the output source of GPO 7. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutStatisticsPulseCount | Number of output pulses. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutStatisticsPulseCountClear | Clears the output signal pulse counter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerOutStatisticsSource | Sets the output source for statistics. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator0Delay | Delay between the input and the output of the pulse form generator. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator0Downscale | Downscale factor at the pulse form generator input. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator0DownscalePhase | Phase for selecting the desired pulse in the sequence. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator0Width | Width of the output signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator1Delay | Delay between the input and the output of the pulse form generator. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator1Downscale | Downscale factor at the pulse form generator input. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator1DownscalePhase | Phase for selecting the desired pulse in the sequence. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator1Width | Width of the output signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator2Delay | Delay between the input and the output of the pulse form generator. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator2Downscale | Downscale factor at the pulse form generator input. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator2DownscalePhase | Phase for selecting the desired pulse in the sequence. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator2Width | Width of the output signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator3Delay | Delay between the input and the output of the pulse form generator. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator3Downscale | Downscale factor at the pulse form generator input. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator3DownscalePhase | Phase for selecting the desired pulse in the sequence. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerPulseFormGenerator3Width | Width of the output signal. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerQueueFillLevel | Fill level of the trigger queue. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerQueueMode | Enables/disable the trigger queue mode. The maximum output frequency is specified by the Trigger Output Frequency parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerState | Sets the state of the trigger system. The state of the trigger system is related to the trigger mode. This parameter enables or disables the trigger processing. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | TriggerWaveViolation | Indicates a distance of two trigger edges violating the minimum edge frequency. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | UncorrectedErrorCount | Number of uncorrected errors. Bit[2] indicates multiple byte errors in CXP stream packets. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | Width | Width of the image ROI on the host side. This parameter is linked with the Width camera parameter. If the camera parameter changes, the host parameter changes accordingly, but not vice versa. The host parameter should not be set to a value different from the camera parameter. Applies to: CoaXPress Visibility: Expert The feature documentation may provide more information. |
![]() ![]() | WriteTimeout | Write access timeout in milliseconds. Applies to: GigE Visibility: Beginner The feature documentation may provide more information. |
PLTransportLayer.AreaTriggerMode Property#
Sets the trigger mode of the area trigger signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.AutomaticFormatControl Property#
Enables/disables automatic control of the pixel format in the device. If enabled, the frame grabber's pixel format and its dependencies are automatically updated to match the camera's pixel format setting.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.AutomaticROIControl Property#
Activates or deactivates the automatic control of the ROI in the Device. If this feature is active, the frame grabber ROI is automatically updated to the camera one.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.BitAlignment Property#
Sets the alignment of the bits in the output format.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.CommandDuplicationEnable Property#
Enables sending all commands and receiving all acknowledges twice. This option should only be enabled in case of network problems.
Applies to: GigE and blaze
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.ConnectionGuardEnable Property#
Enables the automatic start of the PylonGigEConnectionGuard.
Applies to: GigE
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.CorrectedErrorCount Property#
Number of errors corrected. This parameter indicates single-byte error correction in CXP stream packets.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.CustomBitShiftRight Property#
User-defined bit shift to the right. This allows you to shift the pixel data in the output format to the right by a value of your choice. The Alignment parameter has to be set to CustomBitShift for this.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.CxpLinkConfiguration Property#
Sets the link configuration for the communication between the receiver and transmitter device.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.CxpTriggerPacketMode Property#
Sets the trigger packet mode. This parameter allows you to send triggers on rising edges only. It can be used for extreme trigger rates. This parameter may violate the CXP standard.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceAccessStatus Property#
Returns the device's access status at the moment when the Device Update List command was last executed. This value only changes when the Device Update List command is executed.
Applies to: CoaXPress and blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceDisplayName Property#
User-friendly name of the device.
Applies to: CoaXPress and blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceEndianessMechanism Property#
Sets the endianness handling mode.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceID Property#
Interface-wide unique ID of the selected device. This value only changes when the Device Update List command is executed.
Applies to: CoaXPress and blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceManufacturerInfo Property#
Additional information about the manufacturer of the device.
Applies to: blaze
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.DeviceModelName Property#
Name of the device model. This value only changes when the Device Update List command is executed.
Applies to: CoaXPress and blaze
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.DeviceSerialNumber Property#
Serial number of the remote device. This value only changes when the Device Update List command is executed.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceType Property#
Returns the transport layer of the device.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.DeviceVendorName Property#
Name of the device vendor. This value only changes when the Device Update List command is executed.
Applies to: CoaXPress and blaze
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.EventDeviceLost Property#
Returns the unique Identifier of the Device Lost event.
Applies to: CoaXPress and blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.EventNotification Property#
Sets whether the host application is notified of the selected event.
Applies to: CoaXPress and blaze
Visibility: Expert
Selected by: EventSelector
The feature documentation may provide more information.
PLTransportLayer.EventSelector Property#
Sets which event to signal to the host application.
Applies to: CoaXPress and blaze
Visibility: Expert
Selecting Parameters: EventNotification
The feature documentation may provide more information.
PLTransportLayer.FillLevel Property#
Current buffer fill level. This value allows you to check whether the average input bandwidth of the camera is too high to be processed by the applet.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Format Property#
Sets the pixel format of the image that is output to the computer. The data is converted from the internal bit width and color format to the output format selected. This setting is not related to the pixel format input from the camera sensor. For more information, see the Pixel Format parameter documentation.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.FrontGPI Property#
Current input signal levels of all front GPI inputs (bit mask).
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.GentlInfoIgnorefgformat Property#
Ignore the FG output format and manage it internally in the GenTL producer
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.GentlInfoVersion Property#
Version of the GenTL description Interface in the applet.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.GevDeviceGateway Property#
Current gateway IP address of the GVCP interface of the remote device.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.GevDeviceIPAddress Property#
Current IP address of the GVCP interface of the remote device.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.GevDeviceMACAddress Property#
48-bit MAC address of the GVCP interface of the remote device.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.GevDeviceSubnetMask Property#
Current subnet mask of the GVCP interface of the remote device.
Applies to: blaze
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.GPI Property#
Current input signal levels of all GPI inputs (Bitmask).
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.HeartbeatTimeout Property#
Heartbeat timeout value on the host side in milliseconds. This parameter is linked with the Heartbeat Timeout camera parameter. If the camera parameter changes, the host parameter changes accordingly, and vice versa.
Applies to: GigE
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.Height Property#
Height of the image ROI on the host side. This parameter is linked with the Height camera parameter. If the camera parameter changes, the host parameter changes accordingly, but not vice versa. The host parameter should not be set to a value different from the camera parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ImageSelect Property#
Defines which image in a sequence is grabbed.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ImageSelectPeriod Property#
Select the length of an image sequence. Only a single image of the sequence is grabbed.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LinkCommandRetryCount Property#
Specifies maximum number of tries before failing the control channel commands.
Applies to: blaze
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.LinkCommandTimeout Property#
Specifies application timeout for the control channel communication. Up to DeviceLinkCommandRetryCount attempts with this timeout are made before a command fails with a timeout error.
Applies to: blaze
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.LutCustomFile Property#
Filename with custom lookup table values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutEnable Property#
Switch the LUT and processing functionality on or off.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutImplementationType Property#
Type of LUT implementation.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutInputPixelBitDepth Property#
Pixel bit depth at LUT input.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutOutputPixelBitDepth Property#
Pixel bit depth at LUT output.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutSaveFile Property#
Save current LUT configuration.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutType Property#
Enables the LUT to be loaded with custom values or uses the applet's processor.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValue Property#
Field with LUT Values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueBlue Property#
Field with blue LUT Values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueBlueSelector Property#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueGreen Property#
Field with green LUT Values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueGreenSelector Property#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueRed Property#
Field with red LUT Values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueRedSelector Property#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.LutValueSelector Property#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.MaxRetryCountRead Property#
Maximum number of retries for read operations after a read operation has timed out.
Applies to: GigE
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.MaxRetryCountWrite Property#
Maximum number of retries for write operations after a write operation has timed out.
Applies to: GigE
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.MigrationModeEnable Property#
Enables mapping of certain SFNC 1.x node names to SFNC 2.x node names. This allows you to write code for camera devices that are compatible with different SFNC (Standard Features Naming Convention) versions. Available for USB camera devices only.
Applies to: GigE and USB
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.MissingCameraFrameResponse Property#
Returns whether missing frames are reported. If no frame is received for a trigger pulse, the parameter is set to Yes.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.MissingCameraFrameResponseClear Property#
Clears the Missing Camera Frame Response parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.OffsetX Property#
X-offset of the acquisition ROI independent of the camera ROI.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.OffsetY Property#
Y-offset of the acquisition ROI independent of the camera ROI.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.OutputPackedFormats Property#
Automatically outputs packed formats instead of unpacked ones. This parameter is only available if the Automatic Format Control parameter is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Overflow Property#
Indicates whether if the image buffer is currently in overflow state. An overflow results in the loss of images. The parameter is reset at each readout cycle.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.PacketTagErrorCount Property#
Number of packet errors. This parameter indicates that CXP stream packets are lost.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.PixelDepth Property#
Applet-internal processing bit depth. This is the maximum bit depth at which pixels are processed. If you select a highter output and input bit depth, data may be truncated.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.PixelFormat Property#
Sets the format of the pixel data transmitted by the camera. This setting has to match the pixel format set in the camera.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ProcessingGain Property#
Gain correction value. Available when LUT functionality is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ProcessingGamma Property#
Gamma correction value. Available when LUT functionality is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ProcessingInvert Property#
Invert output. Available when LUT functionality is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ProcessingOffset Property#
Offset correction value. Available when LUT functionality is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ReadTimeout Property#
Read access timeout value in milliseconds.
Applies to: GigE
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.ScalingFactorBlue Property#
Blue gain of the white balancing.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ScalingFactorGreen Property#
Green gain of the white balancing.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.ScalingFactorRed Property#
Red gain of the white balancing.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SendSoftwareTrigger Property#
Sends a software trigger pulse or adds pulses to the trigger queue if it is enabled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SensorHeight Property#
Sensor Height in selected tap geometry. Value is ignored if vantage point = TopLeft. Available DRAM and SensorWidth limit the maximum SensorHeight.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SensorWidth Property#
Sensor width in selected tap geometry. Value is ignored if vantage point = Top-Left. Available DRAM and SensorHeight limit the maximum SensorWidth.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SoftwareTriggerIsBusy Property#
Indicates whether the software trigger is busy. This allows you to find out whether the trigger system is still processing software trigger pulses.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SoftwareTriggerQueueFillLevel Property#
Number of pulses in queue to be processed. The Queue parameter needs to be enabled for this.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.StatisticReadWriteTimeoutCount Property#
Number of timeouts during read and write operations when waiting for a response from the device.
Applies to: GigE and blaze
Visibility: Guru
The feature documentation may provide more information.
PLTransportLayer.Statistic_Last_Error_Status Property#
Last error status of a read or write operation.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Statistic_Last_Error_Status_Text Property#
Last error status of a read or write operation.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Statistic_Read_Operations_Failed_Count Property#
Number of failed read operations.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Statistic_Read_Pipe_Reset_Count Property#
Number of read pipe resets.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Statistic_Write_Operations_Failed_Count Property#
Number of failed write operations.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Statistic_Write_Pipe_Reset_Count Property#
Number of write pipe resets.
Applies to: USB
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.StreamDisplayName Property#
User-friendly name of the selected stream.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.StreamID Property#
Device-wide unique ID of the data stream.
Applies to: CoaXPress and blaze
Visibility: Beginner
Selected by: StreamSelector
The feature documentation may provide more information.
PLTransportLayer.StreamSelector Property#
Sets the stream channel. The parameter is 0-based in order to match the index of the C interface.
Applies to: CoaXPress and blaze
Visibility: Beginner
Selecting Parameters: StreamID
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorByteAlignment8b10bLocked Property#
Byte Alignment 8b10b locked
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorChannelCurrent Property#
Returns the Channel Current.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorChannelCurrentSelector Property#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorChannelVoltage Property#
Returns the Channel Voltage.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorChannelVoltageSelector Property#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorCurrentLinkSpeed Property#
Returns the current PCIe link speed in Gibibyte (2^30 byte).
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorCxpImageLineMode Property#
This parameter informs on the current transfer mode, used by the camera. The transfer can be an areascan (= 0) or linescan (= 1) image.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorDisparity8b10bError Property#
Disparity 8b 10b errors
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorExternalPower Property#
Shows the external power state of the board.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorFpgaTemperature Property#
Returns the current FPGA die temperature.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorFpgaVccAux Property#
Returns the current FPGA auxiliary Vcc.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorFpgaVccBram Property#
Returns the current FPGA BRAM Vcc.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorFpgaVccInt Property#
Returns the current FPGA internal Vcc.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorNotInTable8b10bError Property#
Not in table 8b 10b errors
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPacketbufferOverflowCount Property#
Represents the number of overflows, if an overflow occurred due to not correctly aligned package order.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPacketbufferOverflowSource Property#
Represents the port, which has overflows due to not correctly aligned package order.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPcieTrainedPayloadSize Property#
Returns the PCIe trained payload size.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPcieTrainedRequestSize Property#
Returns the PCIe trained request size.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPortBitRate Property#
Returns the port bit rate
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorPowerOverCxpState Property#
Shows the current power over CXP state.
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
PLTransportLayer.SystemmonitorUsedCxpConnections Property#
The currently used number of CXP ports used in this process.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerAcknowledgementCount Property#
Number of trigger acknowledgement packets sent by the camera (in response to trigger edge packets sent before) have been received by the frame grabber.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerCameraOutSelect Property#
Sets the output source to be connected to a camera signal channel.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerEventCount Property#
Number of trigger events sent to the camera.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerExceededPeriodLimits Property#
Returns whether the input signal frequency exceeded the maximum specified. If the parameter returns Yes, signals were dropped.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerExceededPeriodLimitsClear Property#
Clears the Trigger Exceeded Period Limits parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInDebounce Property#
Input debounce time for trigger input signals (in microseconds). This parameter allows you to filter out invalid signals by specifying a minimum signal length.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInDownscale Property#
Factor by which the trigger input signal is downscaled.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInDownscalePhase Property#
Phase for selecting the desired pulse in the sequence.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInPolarity Property#
Sets the polarity of the trigger input signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInSource Property#
Sets the trigger input source for external trigger mode.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsFrequency Property#
Current frequency of the input pulses.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsMaximumFrequency Property#
Maximum input frequency detected.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsMinimumFrequency Property#
Minimum input frequency detected.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsMinMaxFrequencyClear Property#
Clears the minimum and maximum frequency values.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsPolarity Property#
Sets the polarity of the trigger input signal for statistics.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsPulseCount Property#
Number of input pulses.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsPulseCountClear Property#
Clears the input signal pulse counter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerInStatisticsSource Property#
Sets the trigger input source for statistics.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerMultiplyPulses Property#
Upscales, i.e., duplicates, the number of trigger pulses generated externally or via software with the period specified by the Trigger Output Frequency parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutputFrequency Property#
Maximum trigger output frequency. If the internal generator is used, it will use the frequency specified there. If an external source is used, this value determines the maximum allowed value. External trigger signals exceeding this value will be discarded. For more information, see the applet documentation.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectFrontGPO0 Property#
Sets the output source of Front GPO 0.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectFrontGPO1 Property#
Sets the output source of Front GPO 1.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO0 Property#
Sets the output source of GPO 0.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO1 Property#
Sets the output source of GPO 1.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO2 Property#
Sets the output source of GPO 2.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO3 Property#
Sets the output source of GPO 3.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO4 Property#
Sets the output source of GPO 4.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO5 Property#
Sets the output source of GPO 5.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO6 Property#
Sets the output source of GPO 6.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutSelectGPO7 Property#
Sets the output source of GPO 7.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutStatisticsPulseCount Property#
Number of output pulses.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutStatisticsPulseCountClear Property#
Clears the output signal pulse counter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerOutStatisticsSource Property#
Sets the output source for statistics.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator0Delay Property#
Delay between the input and the output of the pulse form generator.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator0Downscale Property#
Downscale factor at the pulse form generator input.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator0DownscalePhase Property#
Phase for selecting the desired pulse in the sequence.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator0Width Property#
Width of the output signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator1Delay Property#
Delay between the input and the output of the pulse form generator.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator1Downscale Property#
Downscale factor at the pulse form generator input.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator1DownscalePhase Property#
Phase for selecting the desired pulse in the sequence.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator1Width Property#
Width of the output signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator2Delay Property#
Delay between the input and the output of the pulse form generator.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator2Downscale Property#
Downscale factor at the pulse form generator input.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator2DownscalePhase Property#
Phase for selecting the desired pulse in the sequence.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator2Width Property#
Width of the output signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator3Delay Property#
Delay between the input and the output of the pulse form generator.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator3Downscale Property#
Downscale factor at the pulse form generator input.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator3DownscalePhase Property#
Phase for selecting the desired pulse in the sequence.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerPulseFormGenerator3Width Property#
Width of the output signal.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerQueueFillLevel Property#
Fill level of the trigger queue.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerQueueMode Property#
Enables/disable the trigger queue mode. The maximum output frequency is specified by the Trigger Output Frequency parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerState Property#
Sets the state of the trigger system. The state of the trigger system is related to the trigger mode. This parameter enables or disables the trigger processing.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.TriggerWaveViolation Property#
Indicates a distance of two trigger edges violating the minimum edge frequency.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.UncorrectedErrorCount Property#
Number of uncorrected errors. Bit[2] indicates multiple byte errors in CXP stream packets.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.Width Property#
Width of the image ROI on the host side. This parameter is linked with the Width camera parameter. If the camera parameter changes, the host parameter changes accordingly, but not vice versa. The host parameter should not be set to a value different from the camera parameter.
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
PLTransportLayer.WriteTimeout Property#
Write access timeout in milliseconds.
Applies to: GigE
Visibility: Beginner
The feature documentation may provide more information.