Threading and Concurrency#
This visualization illustrates how image acquisition works in a Python application.
- Image acquisition runs in a native (C++) thread inside pylon.
- Your Python code retrieves images from a buffer queue.
- This separation enables asynchronous acquisition.
In many applications, image acquisition is faster than processing:
Without concurrency:
- Buffers fill up.
- Frames are dropped.
- Latency increases.
Basic Execution Model#
A single-threaded approach is the simplest form of an image acquisition pipeline.
Example:
while camera.IsGrabbing():
with camera.RetrieveResult(5000) as grab_result:
if grab_result.GrabSucceeded():
image = grab_result.Array
process(image)
This has the following disadvantages:
- Processing blocks acquisition.
- Poor CPU utilization
- Limited scalability
Producer–Consumer Pattern (Recommended)#
This is a more sophisticated approach for an image acquisition pipeline.
- Producer: The acquisition thread grabs images and pushes them into a queue.
- Consumer: The worker threads process images independently.
Example Implementation Using a Custom Thread#
Info
You can use the grab loop thread provided by the InstantCamera (see the grab_using_grab_loop_thread sample). This is a custom implementation for demonstration purposes only.
import threading
import queue
from pypylon import pylon
def process(image):
print(image.shape)
image_queue = queue.Queue(maxsize=10)
# Producer thread
def grab_loop(camera):
while camera.IsGrabbing():
with camera.RetrieveResult(5000) as grab_result:
if grab_result.GrabSucceeded():
image = grab_result.Array
image_queue.put(image)
# Consumer thread
def process_loop():
while True:
image = image_queue.get()
process(image)
image_queue.task_done()
with pylon.InstantCamera(pylon.FirstFound) as camera:
camera.StartGrabbing()
grab_thread = threading.Thread(target=grab_loop, args=(camera,))
processing_thread = threading.Thread(target=process_loop)
grab_thread.start()
processing_thread.start()
grab_thread.join()
image_queue.join()
Queue Behavior and Backpressure#
Strategies:
- Increase queue size.
- Drop frames manually.
- Use
LatestImageOnly.
Combining with Grab Strategies#
LatestImageOnly: Reduces backlog.OneByOne: Ensures completeness.
Best practice:
Thread-Safety Considerations#
- Avoid sharing mutable data without locks.
- Copy images before passing them to other threads, e.g., by using the
Arrayfunction. - Use
queue.Queuefor safe communication.
CPU Utilization#
Parallel processing has the following advantages:
- Better CPU usage
- Separation of concerns
- Scalable architectures
When to Use Multiple Threads#
Use threading in these situations:
- Processing is slower than acquisition.
- Multiple processing stages exist.
- Real-time responsiveness is required.
Avoid threading in these situations:
- Processing is negligible.
- System complexity must be minimal.
Advanced Patterns (Overview)#
Multi-Stage Pipeline#
A multi-stage pipeline splits image processing into independent steps that run concurrently and exchange data via queues.
Multi-Consumer Setup#
Conceptual Pipeline#
Key Takeaways#
- Acquisition and processing should be decoupled.
- Use producer-consumer pattern for scalability.
- Queues provide thread-safe communication.
- Threading improves performance but increases complexity.